AXIS#.SAFEPARAM.SAR_#.FUNCTIONACTIVATION

Description

Indicates whether the Safe Acceleration Range (SAR) safety functions can be activated. One of the following values are used:

Value

Description

0

Never active

1

Read for activation

These functions can only be used when a safe encoder is configured in the safety parameters.

 

Context

For complete SAR information refer to SAR (Safe Acceleration Range).

Related safety parameters:

Versions

Action Version Notes

Implemented

02-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1

Default Value

0 (Never active)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SAR_1.FUNCTIONACTIVATION

3166h

01h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SAR_2.FUNCTIONACTIVATION

3167h

01h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SAR_3.FUNCTIONACTIVATION

3168h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SAR_1.FUNCTIONACTIVATION

3266h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SAR_2.FUNCTIONACTIVATION

3267h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SAR_3.FUNCTIONACTIVATION

3268h

01h

Unsigned8

-

-

Read/Write

No